Hi,
My name is Idan and I'm electronic engineer.
In my application, I need to measure low voltage from serial shunt resistor (0.2Ω) that connected between DC-DC converted from one side (300VDC/ 4A) and a full bridge inverter and parallel big capacitor in the other side (High-side measurement).
For that purpose, I thought to use the INA110 as the first stage and then ISO120SG Isolated amplifier as a second stage (both with ±15V) but in order to do so I need you to clearly the following questions:
- Is it possible to implement this suggestion in a 300V High-side measurement? Do I need a floating power supply reference to the lower leg of the shunt resistor?
- In page 9, COMMON-MODE INPUT RANGE, you mentioned that the differential input signal and its associated common-mode voltage should not cause the output of A1 and A2 (input amplifiers) to exceed approximately ±10V with ±15V supplies. In normal operation that is not a problem because the differential voltage is 0.8V so with fix gain configuration of x10 I will not exceed the ±10V. However, during start up, it is possible that I will have differential voltage of 300V for several seconds(due to the large capacitor) (no common mode due to floating supply).
The question is if I'm using a clamping diode to ±15V (as in FIGURE 14), is the circuit protected (Common mode, differential voltage and so on)? Maybe I need to connect the clamping diode to ~1V (in order make sure that A3 input will not "See" more the ±10V with fix gain of 10).
- In the INA110, FIGURE 14 you mentioned that for high voltages you recommend of R1 = R2 = 100kΩ. Did you mean "high voltages" during normal operation or at overvoltage protection such as start up to 300V? Why do I need such large values? Only to protect the 2N4117A clamping JFET diode?
My second option is to use the AMC1100 amp…
Thanks a lot,
Idan