Other Parts Discussed in Thread: TL062, OPA2364, OPA364, OPA350, OPA365, THS4222, THS4221, OPA211, OPA354, TINA-TI, OPA2354
Hello,
I have an application in which I need to perform automatic gain control. I plan to implement this function by observing the peak of the input signal and using that as my criteria for gain adjustment. I have been successful in implementing the PGA section of the design. However, it is the precision peak detector that causes problems.
Specs:
- Single supply operation +5 or +3.3V
- Input signal's peak voltage may be in the mV to uV
Previous Work:
- Tested with 1N4001 diode (possibly too slow?)
- Using TI's TL062 JFET amplifier (should I use an amp with a different input transistor?)
I would like to know of a circuit using a rail to rail single supply op amp that can put out a half/full wave rectified signal so that I may low pass filter the output to get a peak signal. I can't go with a simple peak detector because it will not rectify the low amplitude signals that I am seeing. Please let me know if you have any suggestions.
Thank you,
Alex