Other Parts Discussed in Thread: AFE031
Hello everybody,
My design is a 24V power line communication. I have set the AFE031 as shown in the TIDU160 PDF from TI... i have connected the AFE031 to 24V (24V IN) and the other pins to 3,3V and 15V as shown in that datasheet... I send from a microcontroller to the DIN pin a sequence of 10bits with a clock signal going to the SCLK pin, doing this:
- Set CS low.
- Set the DAC pin (pin 7) high.
- Write a 10-bit word to DIN.
- CS high updates the DAC.
- set the DAC LOW
the clock signal is 20ms (10ms HIGH and 10 ms LOW) 50Hz..
when i try to read the 24Vin, it has no change and no modulation, it keeps being stable at 24V..
what is happening why i cant see the modulation?
thanks and best regards,
Andres