This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM211 offset balansing

Other Parts Discussed in Thread: LM211

Dear sir, please answer

I'd like to use LM211 with +/- 5V  supply: Vcc+= +5V,    Vcc-= -5V,    EMIT OUT = GND. Can I use offset balansing as shown at the figure 17 of the datasheet?

Please see circuit in attach

R1-R4 is the magnetoresistive bridge (Integrated Circuit  AA004-02). R1 and R4 – are shielded and their value not vary, when magnetic field increase.

R2 and R3 decrease, when magnetic field increase. If magnetic field no, thenR1=R2=R3=R4=5.5k

LM211_.TSC

TIA

Sincerely

Vladimir Naumenkov

www.agat.by