Other Parts Discussed in Thread: LM358
I'm looking at the LM358 for a 12V application. I may have some unintended scenarios on my board and want to make sure the part is protected.
1- What is the max voltage rating on the amplifier output?
2- Looking at the amplifier schematic diagram, it makes me think that if we disconnect power (V+) from the amplifier we will have high impedance on the amplifier output. Is that a correct assumption? If so what would be the max output voltage rating when V+ is disconnected? I'd like for it to have a voltage standoff of 32V.
3- I need to be able to sink and source 45mA at the output. It looks like the sink capability might be a little low on this part. Am I correctly understanding the part's capability?
Might there be a better fit for my application?