Other Parts Discussed in Thread: LM7322
I have a design that uses the LM7322 as a buffer for a voltage reference and as an output buffer that deals very well with the capacitance of the cable and the external circuit. I have an application that requires operation down to -45 degrees C and I wonder if the LM7322 can operate down to below the datasheet limit of -40. I could put the LM7322 through a qualification process but what might I expect to find at -45 or even -55 degrees C? The equipment may only need to start up at -45 as it will heat up during operation.