This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA250 current offset definition?

Hi Team,

Customer asked what is current offset (Ioffset) meant. I am not so sure about it.

Please help to verify if my understanding is correct or not, thanks.

For example, INA250A4: 2V/A, assume 1A go through internal Rshunt 2m ohms, we expect to see Vshunt = 2mV, output will be 2V, so the gain is 1000 v/v.

so 2V = 1A * Rshunt (2m ohms) * gain (1000 v/v). correct?

Ioffset RTI is 20mA at 0A shown in the spec, does this mean if we have perfect Rshunt of 2m ohms, then Vshunt offset = 40mV?  

I believe not, but what does it mean?

Thanks.

Thanks

Andrew

  • Hi Andrew,

    Your first point is correct. 2V = 1A * Rshunt (2m ohms) * gain (1000 v/v).

    Ioffset = Current you will see in the input when no current is applied. Means that Vshunt = 20mA * 2mohm = 40uV ; Vout (due to Ioffset) = 40uV * 1000 = 40mV.

    Regards,