This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adapting THS4524IDBT to THS4541IRGTT

Other Parts Discussed in Thread: THS4541, THS4524

Hello,

Based on below output requirement that the TI OpAmp would receive, how (what resistors & capacitors should be connected in what way) should I adopt the current design to fit the differential input requirements of the ADC (See attached spec)?

Encoder output spec
The input signals can set by a third party into two modes (Amp disabled and Amp enabled), which we need to support. and the vary from below ranges.

XG SCES-Sin-Cos Encoder Scale Single head with differential input signal standard modes:           
Third-party system Amp disabled        2.175V - 2.825V
Third-party system Amp enabled        2V - 3V
The ADC minimum sampling speed is 65Msps and minimum resolution is 12-bit. The amount of simultaneous sampling need is 6 channels (2-axis x A1, B2 & Z-analog encoder signals from motor)

The analog power rail is a clean 5V with plenty of current draw capability (10A).

Please advise.

Thanks,

-albin

Exar_CDK8307_DS-536139.pdf

  • Hello Albin,

    If the input signal is differential then the gain of the FDA is simply Rf/Rg, where Rf is the feedback resistor and Rg is the input gain resistor. For example if figure 73 of the datasheet, the gain is 4.02V/V (ignore C1, C2 and Rm-  not relevant to this discussion).

    Can you please confirm if the input signal in amp enabled mode is 2Vpp differential or 1Vpp differential. The ADC can accept a 2Vpp signal on 0.9V common-mode so I need to figure out whether the amplifier needs to be configured in a gain of 1V/V (0dB) or 2V/V (6dB). Once you confirm this I can send you a TINA schematic showing the resistor configuration.

    Regards,

    Samir

  • Hello Samir,

    Thank you for your reply. It was much faster than expected. :)

    In the "Amp enabled" mode it's 1Vpp (2V-3V). In "Amp disabled" mode it's 0.65Vpp (2.175-2.825V).
    Based on the part number of the ADC, it can go up to 80Msps (with12/13 bit resolution), and the Xilinx FPGA that would receive the output from the ADC can handle both 65Msps and 80Msps. At a minimum we need 65Msps, so additional speed is bonus.
    So, would you be able to keep the current resistor divider and capacitor configuration (Preferred) and just change the values to match the new THS4541IRGTT device?
    Regardless, please also send the accuracy needed on the passive components. The currently used 4.99Kohm resistors have a 1% accuracy, but the rest have 10% accuracy. (Because it's so late in the layout phase I had to change the passive components to 0402 size to make them fit, without changing the PCB size.)
    Looking forward to your answer.
    Thanks,
    -albin

  • Hi Albin,

     I am going to attach two circuits here - one checks the amplifiers loop gain for stability and phase margin and the other one can be used for checking the transient response and the ac closed loop gain of the circuit. As configured the bandwidth is around 92MHz with sufficient phase margin. 1% components would work out well. This will give the lower balance error compared to using 5% resistors.

    I just want you to be aware that when changing from the THS4524 to the THS4541 you will need 4 discrete amplifier channels since the THS4541 is not available in a quad-channel version.

    -Samir

    THS4541_Ckt.TSC

    THS4541_Stability Check.TSC

  • Hi Samir,

    My TINA download, decompressing the ZIP-file and double clicking on the executable works (according to the windows task manager the install launcher is started each time), however nothing happens. No error messages and no window shows up. Starting it in administrator mode or in Windows XP mode gives the same result. I'm running Windows 7 in 64-bit mode.
    I retried download and install it in root directory, but got the same result.

    So, I can't see or use the TSC-files that you've sent.
    Please send the circuits in PDF-version or even better in OrCAD format.

    Thanks,

    -albin
  • Hi Samir,

    I was able to install TINA after PC reboot and simulate the TSC-files. Thanks
    Very sorry. I found out from the Customer that the input frequency has been reduced to max 7MHz, so then I assume we can keep THS4524.
    Please check that the voltage divider before the OpAmp in the schematic is correct.

    Thanks,

    -albin
  • Albin,
    The THS4524 will work in the application now. You can use TINA TI to simulate your circuit and verify if it meets your requirements.
    -Samir