Hi all
The OPA192 has been selected to implement a 0 ...5V and 0 ... 10V output stage and I have two questions:
The temp. range is -40°C ... + 85°C, what supply voltage is needed to guarantee a swing to 5V ( .... or 10V ) respectively ?
The load is 2kOhm and the design is single supply ( ... e.g. 0 / 7V or 0 / 12V).
In the Datasheet on page 11 I find only data for +25°C.
2nd question: The output stage should be able to drive a capacitive load of 22nF.
Input voltage is 3.3V, output voltage should be 5V or 10V.
Can you suggest a suitable circuit that is stable for this value of capacitive load ?
Thank you and best regards
Ue