1. I have application where input signal voltage varies from +5V to -5V. Have to level shift the signal and fed it to microcontroller adc which is sampling at 1MSPS. Microcontroller adc range varies from 0V to 3.3V
2. Selected OPA316 for this application. Attached find the circuit.
Can I level shift the signal using single supply opamp(3.3V) volt from +-5V to 0-3.3Vdc