Other Parts Discussed in Thread: THS4531
Hello,
Referring to the below schematic, I am using a THS4531 to drive a laser diode (D5), whereby a photodiode is providing optical feedback current that is routing through a resistor (R18) to provide the feedback voltage. The reference voltage source is a PWM signal (TP50) passed through an LPF. When the low side switch (NMOS Q16) is active, the laser will turn on. I am observing an instability in the op-amp output shown in the following scope plot. The laser diode current is < 10 mA and the system supply voltage is +3.6 VDC (single supply). A 0.01 uF ceramic capacitor resides near the op amp between the supply and ground.
Op amp output: Blue; Photodiode return (TP49)n: Green; Q16 gate (TP48): magenta
Any insight as to what may be causing the undesired oscillations is appreciated.
-Andrew