I want to amplify a square signal, whose amplitude is 400 mv, and frequency is 200 khz. And I used the LM4250, the circuit diagram is shown below:
I connect the square signal to the positive input, and connect v- to the ground. I connect the pin 8(Quiescent Current Set) to a 1M ohm resistor. And V+ connects to 5 v. However, there is no output voltage and signal at all(detect with oscilloscope). However, when I change the AC input signal to DC signal(input voltage is 1 v), keep other setting the same, and I could detect the output voltage is equal to 4.5 v. So I don't know what is wrong with my circuit and how to solve this problem? And does this pin 8 necessary and do I need to connect pin 8 to any resistor?
Thanks very much.