Other Parts Discussed in Thread: INA300, TIDA-00795
Hello,
I am working from the eFuse design using INA300. The alert signal does not pull low once the load current goes above the set load current. I am using a 7500ohm resistor at the limit pin to correspond to a 150mV reference voltage. However the voltage at this pin is 75mV. Also the voltage across the sense resistor is half of its expected value at a given load current. This would be fine since the Limit voltage is half of its expected value only the Alert pin does not trip when the voltage across the sense resistor is above 75mV.
I am using a 30mohm sense resistor and a maximum load current of 5A.
Could you please help with this problem? If you require information please let me know.
Thank you