This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2188 Long-term stability

Guru 20090 points

Other Parts Discussed in Thread: OPA2188

Hello,

In the OPA2188 datasheet, there is the long-term stability specification as 4uV(typ) and there is the note (1) of "1000-hour life test at +125°C demonstrated randomly distributed variation in the range of measurement limits—approximately 4 μV".

Is this mean 4uV/1000hour(typ) ?


Best Regards,
Ryuji Asaka

  • Hello Ryuji,

    As part of the product qualification process, OPA2188 was life-tested for the equivalent 1000-hours operation at 125°C temperature and it passed the maximum allowable Vos shift limit of +/-25uV; what this means is that the typical part with the initial Vos =5uV may typically shift after 1000 hours of constant operation at 125°C by +/-4uV, thus ending up at either 1uV or 9uV (5uV+/-5uV).

    Best,

    Errol Leon
    Precision Op Amp Applications
  • Hello Leon,

    Thank you.
    I understood that the Vos shift is +/-4uV/1000hour at 125C operation.

    Best Regards,
    Ryuji Asaka