Other Parts Discussed in Thread: OPA381
Hello,
I am looking to design an analog front end similar to the input of an oscilloscope. I have been able to get a simulation working in TINA TI, but the design is *not* single supply and requires numerous components and exotic voltages (-2.5V, etc).
The requirements are as follows:
1) Single supply operation (+5V or +3.3V are acceptable)
2) Must present input impedance of 1 Mohm and ~25pF
3) Needs to have an analog bandwidth of 1 MHz
4) Must have AC/DC coupling option
5) Needs to accommodate over voltage conditions
The current design's block diagram looks like this:
Input (Probe) -> AC/DC switch ->Attenuator (resistor and capacitor divider circuits) -> Level Shifter (for single supply operation/ADC range matching, I am unsure how to do it)-> Input diode clamp -> Following Op Amp (OPA381) -> Gain Stage (undecided as of now) -> Anti-alising filter (undecided, but probably needs to be 2nd order) -> ADC
I am primarily looking for suggestions as to how I could create 100% single supply version of this system. I have seen other circuits that do level shifting in the attenuator stage, but they did not seem to simulate well in TINA TI.
Thank you,
Alex