Other Parts Discussed in Thread: PGA280
If supply power to the PGA280 if off (VSN = VSP = 0V) can voltage be present on the inputs without damage. For example, if the power to the part is off and a +- 2V sine wave is present on the inputs, how will this impact the PGA280? This has happened repeatedly in some testing and the part seems to continue to function well without issues but I would like to confirm that this situation is OK.
Thanks