Hello,
I have an application that requires to sense the amount of light coming into multiple photodiodes for material recognition. To get a faster speed and to get the most linear output range i'm going to need to use a transimpedance amplifier with the diode reverse biased. Get a direct current to voltage conversion.
But putting a current to voltage amp on every photodiode is not practical due to cost and space. I was wondering what would be the best way to multiplex each photodiode to the same transimpedance amp? Sense the amp needs to directly measure the current through the diode I'm not sure how putting analog switches between the diode and the amp would affect how that works.
I know the multiplexer would affect the bandwidth, noise, error, but that would be ok as long as the final system is within the bandwidth I need. I need to know if the whole principle of the current to voltage conversion still applies even when going through a mux of some kind.
Is the linearity of light energy in to voltage out going to be as good?