Hi,
I am using LMH6321 to drive my trigger signal of 8V , i need to drive around 30 m 50 ohm cable with load of 50 ohm. if i use the sample circuit as suggested in datasheet, R4 (50 ohm) resistance is used in series to compensate the capacitance of coaxial cable but output voltage decreases to half in this configuration. What should i do to keep the output voltage same as input voltage and drive it to 30m also.

Regards,
Mukund Jha