Other Parts Discussed in Thread: OPA333, TLV369, OPA369, OPA2333, TLV379
Hi all!
I'm currently working on an optimized low current measurement circuit.
The inspiration is coming from the ucurrent sensor found here: https://www.eevblog.com/projects/ucurrent/
However, our problem is very specific:
1) Supply voltage is 2.5V
2) I need one OPAMP to create a virtual ground @ 1.25V (2.5V / 2)
3) I need one OPAMP to amplify the voltage generate bu the current passing by the low value resistance. (mucurrent has two but if we could do with one it's better)
In our case, we would like to have an output of 0 to 2.5V output by having a current of -500ma to 500ma into a 0.1ohm resistance. This means an amplification of 25. For this, a simple non-inverting circuit is doing the job.
4) It's going to be AC current with max 60 hertz frequency where we will only sample few cycles to get maximum and lower value on a given cycle.
and we have one constraint:
5) Consumption must be as low as possible
To sum it up, I need two OPAMP for two different features: virtual ground @ 1.25V (gain of 1) and 25x (gain of 25) amplification of voltage across resistance due to current.
Is there one type of OPAMP who could do both with very low consumption and 2.5V supply? Or do I need two references?
I'm trying to read specs and I'm getting a bit lost on which one to choose. Could someone guide me just to make the right choice?
Thanks for you help!