Other Parts Discussed in Thread: OPA354, LM358, OPA171, OPA172, LT1013
Looking for a single supply op amp capable of 0 to 10V output. Its output should get to within say 10 mV of ground when input is 0 V. This would be for a load of say 10K. The OPA354 has worked well for me but is only a 5V device. The LM358/324 can get that close to ground but I am looking for a better quality op amp.