Other Parts Discussed in Thread: DRV425, DRV425EVM
I would like to measure 4-20mA process current by passive means (without disconnecting wires). The inductive clamps that I have seen are expensive. Is there a TI inductive device that I can consider that would get me the required resolution (4.01mA for example) to two digit accuracy past the decimal? This clamp (or other)arrangement would be connected to a data logger. I don't mind building a circuit or doing some microcontroller programming. It would be nice to get the output signal in mA.