Hi
I have interfaced OPA333 directly to a full bridge load cell. I have added a small positive voltage at the negative terminal of the opamp to keep the o/p voltage within 500 mv.
Now when I vary the temperature from 24 degree centigrade to 60 degrees what I observe is the output of opamp changes. Following are the observed results.
25 degrees 510 mv
35 degrees 498 mv
45 degrees 508 mv
55 degrees 508 mv
As observed the output changes from 25 degrees to 45 degrees is this expected.
Kind regards
Suchitra