Other Parts Discussed in Thread: OPA317, OPA2317
Hello team ,
some of my customers are using the circuit attached below as a bi directional current sense
Inverter_current_monitor.TSCBasically each op amp gives voltage across the rsense in half cycle
outputs of these op amps go to the uC where they are read
in my conversation with BU , it was pointed out that this architecture would violate the Absolute maximum ratings of the input pins of the op amp
However due to the high value resistance connected at the input the current flowing through the internal diodes is limited
Can you please help me understand more about this architecture , and if we are indeed violating the input absolute max specs can we modify it slightly to make it acceptable
Thank you