I would like to know if it's possible to configure the LMP91000EVM's sampling rate. Preferably, obtaining a sample once every four seconds, which would be slow enough as to not create a huge text file from testing over the span of a day or two.
This question has also come to mind because the LMP91000 software that's tied with it does not seem to run longer than a couple of hours (17,000-31,000 seconds). My hypothesis is too much data has been collected for the program to handle, which would mean a smaller sampling rate would lengthen the time the program can run.
My hope is that this post gets some acknowledgement in the form of an answer or advice. I appreciate it very much.