Hi team,
we got following request about ISO124U :
"..one customer wants to use ISO124U for a high-voltage industrial application and he has some doubts regarding technical specifications.
Looking at the data-sheet, the rated Vrms voltage is 1500 V so no problem at this point.
Looking at the Test Conditions on page 5 you specify 2400 Vac during 1 second but the customer needs to test the behaviour applying 2000 Vac during 60 seconds. Is the expected life-time reduced after the test?
The customer also needs to implement a surge peak test applying 5 kV during 1 microsecond. Is it possible to do so ?, is the expected life-time affected during this test ?.."
Thanks in advance for for kind help/suggestions and BR
Sergio