Other Parts Discussed in Thread: TLV3701
I have a customer who is seeing the following:
We are currently using the TLV3701IDBVR comparator. When we startup the comparator with 3.3V it outputs a logic high (for 300us to 2400us) even though the negative input is driven high and the positive input it attached to ground. Additionally the power on time seems to vary widely based on the power down duration.
There are two scope shots that he sent:
CH1 = In+
CH2 = In-
Ch3 = Vcc
Ch4 = Output
The time frames in the scope shots are different. He explained it below:
The only difference is the time I waited between powering up the IC from the last power down. If I wait only 5 sec, I will see a longer time (2.4ms). If I wait 30 sec, I will see a shorter time (200us).
This seemed to imply to me that there was a large capacitive load. He describes the load below:
There are 3 IC that are on the load with no additional capacitance. The load is high impedance (>10M). The issue has been seen on 2 of 2 boards that we checked.
I do not understand how this is happening. Is there something internal to the IC that takes a certain time span before it outputs the proper output voltages based on those present at the input. The output does become proper, but shouldn’t it do this when it powers up also.
Please let me know if you have further questions for the customer.
Thanks for your help with this!
Richard Elmquist