Hi sir
we choice TLV521 to as a comparator due to low cost, small package, low power nanopower and circuit as below.
Is there something we need notice? and TLV521 seems have no Hysteresis spec. is it suit to be comparator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Chen,
The TLV521 is an operational amplifier, not a comparator, so it would not have a hysteresis specification. Internal hysteresis would not be good for an op-amp.
The TLV521 can be used as a comparator, but external hysteresis needs to be added.
Op-Amps generally make poor comparators, and we generally discourage the practice, but there are situations where they are suitable.
Beware, that without hysteresis, the output will chatter as the input slowly approaches the threshold. An op-amp, since it has a linear (not digital) output, can oscillate or float at some random voltage between 0 and 3.3V.
See the following blogs:
https://e2e.ti.com/blogs_/archives/b/thesignal/archive/2012/03/14/op-amps-used-as-comparators-is-it-okay
https://e2e.ti.com/blogs_/archives/b/thesignal/archive/2013/01/28/comparators-what-s-all-the-chatter
Also see AN-74. While it is about the LM339, the hysteresis concepts are the same:
http://www.ti.com/lit/an/snoa654a/snoa654a.pdf
The op-amp has a push-pull output, so it does not require the pull-up resistor (R80).
Regards,