This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NE5532 output short circuit

Other Parts Discussed in Thread: NE5532

Hi,

Let me confirm about behavior of following case.

According to datasheet of NE5532, above spec is described.

I understood that this spec mean maximum current which OPAMP can output (In other words, even if the circuit is short, OPAMP output up to 60mA(worst case is 10mA)).

So, I believe that following behavior will be observed in following case. Is my understanding correct ?

* When output short-circuit current is 10mA(worst case) and output is required 15mA, offset will be appeared on output.

Best Regards,

Machida