Other Parts Discussed in Thread: AMC1100, ADS1014
I am using the AMC1100 in an industrial instrumentation device and I am generally very impressed with the product (Survived 7kV surge testing in my circuit)
We have observed something odd though. In the attached circuit the AMC1100 are exhibiting a gain of around 8.3, We have had 5 prototype boards made from the same batch of chips, and they all display the same behaviour. Luckily for me the ADS1014 that sits downstream of the AMC1100 can sample up to the 3.3V supply rail, so I still make the product spec in terms of usable range. There seems to be no other issues. Linearity and offset both appear within spec.
Our scope is not very accurate, so the following readings were taken at DC using a stable power supply and a calibrated volt meter.
Short the AMC1100 input together, measure the differential output offset. We read 6.3mV, high, but in spec.
Apply +100mV across the inputs. Expecting 806.3 mV at the output, however we get 836mV,
Apply -100mV accross the input. Expecting -793.7mV at the output, however we get -824mV.
Supply rails are correct and stable.
Any ideas? There is simple LPF between the AMC1100 and the ADS1014. The minimum input impedance of the ADS1014 is about 70k Ohm.