Other Parts Discussed in Thread: OPA140, OPA197, OPA191, OPA192
I'm using a single gain AD8605 (Supply 5V) and an OPA140 as a non inverting 50x amplifier (Supply: +%/-5). Both positive inputs are tight together. Small signals are amplified by OPA 140 while higher levels are routed through the single gain amplfier into a different ADC input. In front I have a 10k resistor for current limiting purpose when something goes wrong. With higher voltages (approx. 2.5V at the pos. input) I see a significant current in the pos. input of opa140 (voltage drop at 10k resistor).
Does the opa40 has something like antiparallel diodes between the inputs without notice in the docs?