I have a TLE2082CP, and my power supply is +24 volts DC. I see on the data sheet this works off +/- 5 VDC and/or +/-15 VDC. So is that +15 VDC on the Vcc+ and -15 on the Vcc-? If so thast voltage drop across the two is 30 VDC. So could I power this op amp with +24 VDC on Vcc+ and 0 VDC (command/ground) on the Vcc-? Or do I need to go through a voltage divider to get +15 VDC for the Vcc+ pin?