This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPAx316 as Buffer for ADC Common Mode biasing



Hi team,

I'm looking for a way to drive the Common Mode for an ADC.  We're looking to drive 875mV @ 4mA to set the common mode on the ADC input pins.  The device should also be able to drive a cap load of 0.8uF, which is fairly large.

I was looking at the OPAx316 for this, but due to the size of the capacitive load I believe I must compensate the circuit.  I would be using the Op Amp in a buffer configuration from a resistive divider input.  I think perhaps I'll need dual feedback and an isolation resistor.  Could you help me with the circuit design for this application?  

Thanks,

Kareem