Part Number: XTR117
Other Parts Discussed in Thread: XTR116
Hi,
I used the XTR117 integration in 4-20mA 2-wire transmitter circuit. I used the regulator output of the XTR117 to supply the microcontroller. According to the source current from XTR117, there are voltage differences at the output of the regulator, and this causes a problem for the loop current values.(because of the MCU PWM voltage value).
How can i fix this problem? Can we use the XTR116 and switch(PWM) the Vref output with the transistor, and connect to the current input of the XTR116?
Thanks.