Other Parts Discussed in Thread: AMC1200
hi everyone,
I am following this app note to use the AMC1100 for input voltage sensing off mains: http://www.ti.com/lit/an/slaa552/slaa552.pdf
Specifically, I have built up this circuit here and had it fabbed on a PCB (no breadboard) and am now testing it out:
When looking at the output at 'ACMAINSENSE' I am seeing a signal much smaller than what I would expect for the gain of 8x. My questions are:
- is the app note correct to leave the VOUTN completely un terminated?
- i am using a 5V supply on the isolated side instead of 3.3V in the app note. would this make any difference in the application?
- i am omitting the zero cross detector in favor of a buffer op-amp to then send the analog voltage to an single-ended ADC that is muxed with many other sensor signals. would it be better to receive the output of the AMC1100 with an op-amp differentially?
This is my first use of an isolation op-amp, so I apologize for any oversights on my parts.
Thank You,
Mike
Thank You!