Part Number: OPA657
Hi,
I'm using the OPA657 as a high gain transimpedance amplifier. While it works well with split power supply rails, I want to use them with a single supply so that I can control them using TI's load switches.
To do this, I connect Vss to GND, and Vdd to +10V. However, the output I see on the scope is incorrect. In fact, I also see that the amount of power consumed is half of that with a split rail, which makes me think that I might be missing something. Is there anything else I should be doing to ensure correct operation with a single supply? (I imagine I am within the ICMR since my Vin+ is connected to gnd as it is, which would make the CM on Vin- also be 0V. )
Any help would be greatly appreciated!
Thanks,
Ajay