Part Number: OPA191
For a new design, I have to include the measurement of the sonde pressure level (frequency range between 2 - 250 Hz).
The output of the microphone is modulated on a DC component (around 13 VDC).
Before the AD converter I have to remove the DC component. For that I use an active high pass filter.
The cutoff frequency of the filter is <1Hz.
I have a problem of wave on the output of the filter.
Because the values of the capacitor and of the resistor are quiet high (1uF for the capacitor), do they have some precaution to take ?
For example, is it possible to use a ceramic capacitor X7R ?
We often use NOP or COG for filter but the value are too low with this technology.
The used amplifier (OPA191) has a low bias of 5pF. Do you think it could be a problem ?
Any hint will be appreciate.