This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2902: Absolute max value of INx pins

Genius 17535 points
Part Number: LM2902


I have a question for LM2902.

 

Absolute max of INx pins is defined as absolute value(-0.3 - 26V), not respected to Vcc.

Is it really OK to input some voltage on INx pins when VCC=off?

 

Regards,

Oba