Hello,
Now we are using the INA226 to measure the current by using 20mohm+/-1% shunt resistor in design. We have two questions about it.
1. How to get the current accuracy according to INA226 datasheet in theory?
2. When we do current measurement for a constant current source, we find the measurement value will be slowly increased over time. For example, measure the 3A@5V. The measurement value will change from 3.024A, 3.025A, 3.026A, 3.027A ...... and so forth.
So could you help to respond to above questions?
Thanks,
Best Regards,