This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91000: Using AFE with analog mux

Part Number: LMP91000


Hi,

Can I use two lmp91000 together that  RE and CE pins connected to a sensor via multiplexer? I mean, I`m planning to bias sensor with two chip, one at a time, RE and CE pins of first LMP91000 will be selected via analog multiplexer, then at another time, RE and CE pins of the second chip will be selected. Do that cause any delay, spike or etc. ? I`m planning to do that switching processes several times in a second.

Thanks.