Part Number: INA301
Hi everyone,
I am developing a precision current source using the INA301A1, but am running into some pretty significant issues. One of my biggest problems is that the gain on the device is specified to be 20 V/V with a maximum error of 0.1% but I am seeing errors in gain as large as 9%.
Has anyone had a similar experience or know what it could be caused by. I have attached the schematic for the control loop. The output of the current sense amplifier is feeding the input of the DAC. I have also removed the load voltage sense circuit since it contains an error. I have removed the DAC and still get a significant gain error from the INA301. I am also testing this with a 1k resistor across the load pins.
Thanks,