Part Number: VCA822
Hi,
I'm implementing a Voltage Controlled Amp using a VCA822. I have got two ICs, each time I connect and power them up to +/- 5V and GND the ICs over-heat to the point I am afraid they will be destroyed. There is no mention of any configuration in the datasheet that would cause this. Is there something I am missing? This also happens when I configure the IC into the basic test circuit in Fig 77 in the data sheet. I'm driving the Rg with a 10K pot and injecting a 8KHz signal from a generator into Vin.
Regards
Phil Thomas