Other Parts Discussed in Thread: LMH6703
Hi folks,
I'm Designing a high slew rate DC electronic load in which a voltage feedback operational amplifier is driving a power MOSFET (Varying its resistance in the saturation mode and dissipating heat) .The main objective of this
work is to design a high slew rate load (current Sinking).
I have two doubts Regarding the above.
1.Will the Input Control Voltage Slew rate across Op-AMP determine the Output current slew rate Through MOSFET
2.Do we need a Saturation mode Gate driver to achieve the above objective.
and is there any FET Drivers available(That operates MOSFET in Saturation region).
What I believe is Driving the MOSFET with just Op Amp will not yield the required high slew rate (since the input current of the FET is not sufficient to Charge the Input capacitance of
the MOSFET .
Correct me If im wrong and thank you in Advance
Regards
Manjunath I