This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC555: ERROR ON THE TLC555 DATASHEET

Part Number: TLC555


TI Engineers,

I hope you will agree that there is a mistake on yourTLC555 datasheet in the VOH section.

Please see the datasheets below.

Please let me know that this is indeed is a mistake on the 555 datasheet.  I need a corrected TI datasheet or at the very least, the correct binding specification from a TI engineer so I can proceed with my project.

Thank you.

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • Hi Steve,

    Yes, that is an error in the TLC555, VDD = 5 V table. The IOH current level should be -1 mA, not -1 uA, for the VOH specification. It appears that the error happened with the 2016 datasheet revision.

    I'll let our Marketing Engineer know of the error.

    Regards, Thomas

    Precision Analog Applications Engineering