Part Number: RCV420
Hello everyone!
I am using rcv420 for (4-20mA) current to voltage conversion in this configuration shown in the image.
I am using two different sources one(+-12 V) to power up the rcv420 and other (+15V) to drive current through a variable resistor as my current source. The problem is that I am getting an offset of about 1.25 Volts for 4 mA current and similarly for 20 mA I am getting 6.27 Volts. The output goes zero for 0 mA. Please help me if I am using it correctly or what changes do I need to make in order to null the offset and get 0 to 5 V corresponding to (4 to 20 mA)
Thanking you in anticipation.
Regards,
Muhammad Awais
Student at QAU, Islamabad.