This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Requesting for Low noise Single channel Op AMp

Hello,

I need to connect my Microphone output to Controller over a distance. so i need to add amplifier circuit. My present Amplifier circuit is using the part numer ADA4841 as it is recommended by application note of Microphone. Could you please provide a replacement for ADA4841 which has same specifications and Low cost.

  • Hello Kiran,

    The closest match regarding noise performance to the ADA4841 would be the OPA1611. I also recommend taking a look at the TLV171 for microphone applications and also searching through our audio amplifiers which you can find here. Please let me know if any of the options I provided will work for you.

    Thank you,

    Tim Claycomb