Part Number: OPA191
Other Parts Discussed in Thread: OPA188, TLE2061
Hi,
Do you have a -55C operating part number for OPA191?
Thanks
Shihab.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Shihab,
I did a search of the TI products and did not find a version of the OPA191 that is specified with a -55 C low end operating temperature; -40 C is its lowest temperature. Would the OPA188 be a consideration? It is specified with a -55 C operating temperature and has similar electrical specifications.

Regards, Thomas
Precision Op Amps Applications Engineering
Thanks Thomas for the reply,
I was trying to get a replacement for TLE2061MD. OPA191 has lesser quiescent current spec compared to TEL2061. Also it can drive high loads.
Can you provide an op-amp which has following spec.
GBWP: ~2.5MHz
Power supply : +/- 15V
Temp range: -55 to +125C
Quiescent current: <390uA
Output drive: 20mA (over the operating temp). output swing should be capable of with in 1.5V of the power supply rails.
Reduction of Aol with respect to loading should be better than TLE2061.
Thanks,
Shihab.