This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA172: OPA172 Differential Output Impedance Looking In Calculation

Part Number: OPA172
Other Parts Discussed in Thread: TINA-TI

The OPA172 is connected in a constant current source configuration. I'm having a hard time understanding what the impedance will be when measuring between R3 at 10kHz. If you measure the impedance between R3 at 10kHz, will the impedance be:

Output Impedance of Opamp at 10kHz (1 ohm) to ground,

up R1 from ground (100 ohms). Total impedance at 10kHz is 101 ohms at 10kHz? 

  • Hi EE_Matt,

    The impedance looking to the left across R3 will be 100k for low frequencies up to ~1kHz where loop gain is large. Beyond this frequency, the circuit's loop gain starts diminishing and the impedance lowers as a result.

    At 1kHz, loop gain is 20dB (loop gain = (10MHz / (1+(100k/100))) / 1kHz = ~10V/V = 20dB) and it's down to 0dB at 10kHz. 10MHz is the OPA172 Gain Bandwidth product and (1+100k/100) is the applicable noise gain for this circuit.

    Here is an estimate of the output impedance looking to the left showing 71.1kohm:

    Here is the TINA-TI simulation file for reference:

    OPA172 Output Impedance E2E Hooman 1_23_17.TSC

    Regards,

    Hooman

  • Thank you, this was really helpful.