Part Number: OPA615
Hi everyone, I met some problem when I build the circuit to test OPA615.
I only want to use the OTA function not SOTA part. Therefore, I just leave the pins(4,7,10,11) related to SOTA part disconnected, and build the others just as figure 39 in datasheet. In addition I connected Pin 2(Emitter) directly to the ground. For pin 12 (Collector), I used a resistor of 50 as the load.
However, when I powered this chip without injecting input signal, I noticed that there was some DC value at the input pin (Base) and the output pin (Collector). For different chips, the value will be different.
In addition, for one chip, it turned out quite confused condition, which is there are quite large current flowing out of the power supply, around 150mA. However, after I injected a input signal like 30mV with a 25 resistor in series at the input pin(Base), that chip turned out to work properly.
My question is:
First, how to deal with the unused pins for SOTA part, so that there is no impact on my OTA function part.
Second, where is the DC value from under input pin open circuit? In addition, why there is a big current flowing in the chip?
I wonder if the chip cannot be used as the input pin is under open circuit.
I am looking forward to your reply. Thanks so much.