Part Number: INA220
Hi,
I have a question about the INA220 application.
If I have one I2C bus with three INA220 as slaves, can I trigger each of them without stop sign in the coding in a interleaved way? I want to read out the information from three power monitors in an interleaved way while I want to update the power information in these power monitors every 5ms without the stop sign leading timeout (28ms). Otherwise, the power monitor will be frozen for a long period of time without updating the new information.
Best
Yu Geng