Hi,
Piezo-electric sensors present a very high impedance small-signal voltage or charge source. Typically, a differential signal is inputted to a discrete pair of matched ultra low-noise JFETs, biased with a current mirror. I am wondering if there is a IC op-amp approach available today, that does not require very large resistors, and is ultra low-noise. My application requires a modest bandwidth of 25 - 1,500 Hz and low slew rate. I can tolerate input offset voltages of up to 20 mV. I am constrained to use a single ended supply of 0 V to up to 15 V.
Thanks,
Paul Lander